AXIS#.PL.KP

Description

AXIS#.PL.KP sets the proportional gain of the position regulator PIDClosed"Proportional-Integral-Derivative" A PID controller is a generic control-loop feedback mechanism widely used in industrial control systems. An "error" occurs when an event or a disturbance triggers off a change in the process variable. A PID controller attempts to correct the error between a measured process variable and a desired setpoint by calculating and then outputting a corrective action that can adjust the process accordingly loop.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Hz

Range

0 to 500

Default Value

3.27

Data Type

Float

See Also

AXIS#.PL.KI ,

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.PL.KP 0x500C 0x4 UDINT 1000:1 - RW False
AXIS2.PL.KP 0x510C 0x4 UDINT 1000:1 - RW False